Skip to main content
Visitor II
January 17, 2007
Question

Is there IAP example code available?

  • January 17, 2007
  • 3 replies
  • 904 views
Posted on January 17, 2007 at 05:12

Is there IAP example code available?

    This topic has been closed for replies.

    3 replies

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:35

    I need program Bank0 from Bank1.

    WBR,

    Dawei Shang

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:35

    Hello shangdawei,

    Yes, ST will provide a driver allowing programming the STR91x Internal Flash Bank0 using In Application Programming via UART.

    The IAP driver is to be programmed by the user in the Flash bank 1 after being hardware remapped at address 0x00 (bank 0 is hardware remapped at address 0x80000). Programming is performed via JTAG using a flasher toolset.

    Using the UART, the IAP driver loads a binary file from HyperTerminal to the STR9 internal Flash bank 0, and then jumps to execute it.

    More details will be provided in the ''STR9 In-Application Programming using UART'' application note which will be published on the web few days later.

    Best regards,

    Najoua.

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:35

    Hello again shangdawei,

    Now, the ''STR9 In-Application Programming using UART'' application note (AN2475) and its corresponding software are available on the following web link:

    http://www.stmcu.com/modules.php?name=mcu&file=familiesdocs&FAM=101

    Best regards,

    Najoua. :p