Skip to main content
Visitor II
March 5, 2008
Question

Is this another Bug in the NEW FWLib for the SSP?

  • March 5, 2008
  • 1 reply
  • 595 views
Posted on March 05, 2008 at 20:15

Is this another Bug in the NEW FWLib for the SSP?

    This topic has been closed for replies.

    1 reply

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:32

    Where is SSP1? Comment says 0 or 1

    Where are the Code reviews?

    With all these bugs we should get free support forever!

    Motorola gave me free support many years ago for finding many of their bugs!

    /*******************************************************************************

    * Function Name : SSP_DeInit

    * Description : Deinitializes the SSPx peripheral registers to their default

    * reset values.

    * Input : SSPx: where x can be 0 or 1 to select the SSP peripheral.

    * Output : None

    * Return : None

    *******************************************************************************/

    void SSP_DeInit(SSP_TypeDef* SSPx)

    {

    if(SSPx == SSP0)

    {

    /* Reset the SSP0 registers values*/

    SCU_APBPeriphReset(__SSP0,ENABLE);

    SCU_APBPeriphReset(__SSP0,DISABLE);

    }

    }