ISO808 Ground connection

in ISO808 I have connected +5V at VDD and +28V at VCC. In my application isolation is not required so is it ok if I short GNDDD and GNDCC with filter?

in ISO808 I have connected +5V at VDD and +28V at VCC. In my application isolation is not required so is it ok if I short GNDDD and GNDCC with filter?
For example, you could use the VNI8200XP, which has OUT_EN but can only be used via SPI because OUT_EN is shared with IN3. Otherwise, you can stay with the ISO808.
If the problem is solved, please mark this thread as answered by selecting Accept as Solution, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.