I use ST7MDT2-DVP2 to program St72C334N4T6 by using ISP. First I can program the programm area(I forgot to program the option byte) and then the program can work. But now I can not program with ISP. I don't know why? I measure the Reset pin and ISPSEL pin and found that the Reset Pin is OK and I can see 33 clock on ISPSEL pin but the bottom level of ISPSEL is about -1V. the voltage of ISPCLK and ISPDATA pin is always 0V. could anyone help me? Thanks a lot!