Issue with Reading Back Values on VNF1048F IC
I'm having trouble when reading back the values I have written to the VNF1048F IC.Every time, the unused bit is being enabled, Even after only performing the software reset,the unused bit is setting.Here's what I have tried so far:
1.Performed a software reset.
2.Set the Unlock bit and write unlock bit threes times in control register3
3.Set the watchdog trogger to 1 and the watchdog time to 200ms.
4.Enabled the EN bit.
5.Configured the threshold values.
Despite these steps,when i read back,only the unused bit is being set, and no other bits are enabling.Can you please help me to identify what might be going wrong?