Skip to main content
Visitor II
August 1, 2006
Question

JTAG registers of stacked-flash

  • August 1, 2006
  • 5 replies
  • 1095 views
Posted on August 01, 2006 at 08:04

JTAG registers of stacked-flash

    This topic has been closed for replies.

    5 replies

    bastianAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:30

    Hi,

    I'd like to try to erase my flash using jtag. But so far

    I did not find any infos about the jtag commands.

    Anyone got a link ?

    Edited:

    Found it on the st912 page. Now trying if I can get on the flash using j-link.

    [ This message was edited by: 42Bastian on 28-07-2006 17:26 ]

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:30

    Hi,

    There is a seperate STR9 flash programming manual available from this website.

    Martin.

    bastianAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:30

    �es, found it.

    Now , as I wrote, I have to figure out how to attack it.

    My only device I have is a J-Link with some SW. But so far I don't

    seem to have the correct codes sent. I even do not get the IDCODE.

    My computer has no parallel port anymore, so the ST JTAG solution

    does not work.

    I am close to using another ARM board :)

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:30

    What software are you using with the JLINK, is it not IAR ? Perhaps you are using the free gdb server available on the net.

    The jtag config of the str9 is as follows:

    3 taps are present, scan chain (ir 5 bits), arm966 core (ir 4 bits) and flash controller (ir 8 bits).

    I have added support to Openocd for the str9 and this should be available in svn very soon.

    Also the str9 (arm966) is a strange beast, the monitor mode is enabled at reset ? unlike other arm9 cores. This has to be disabled before breakpoints etc can be enabled.

    Regards

    sjo

    bastianAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:30

    I downloaded a SW collection from segger.

    Anyway I will look at openOCD.

    I meanwhile als tried iSystem, but so far I have no luck in getting anything meaningfull

    back from either my str9 nor from a LPC2294.

    I am really close to writing my own tool.