Skip to main content
Visitor II
July 25, 2007
Question

Keil write COULD NOT STOP ARM DEVICE

  • July 25, 2007
  • 15 replies
  • 2079 views
Posted on July 25, 2007 at 06:20

Keil write COULD NOT STOP ARM DEVICE

    This topic has been closed for replies.

    15 replies

    k_arthurAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:40

    I have tried uploading from bank 1. I forgot to set bit in the STR9xCFG.s file.

    Now i can not reprogram the STR911.Keil write COULD NOT STOP ARM DEVICE.

    Anyone knows how to correct this?

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:40

    http://www.keil.com/support/docs/3215.htm

    try this

    k_arthurAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:40

    I tried to do steps writen on

    http://www.keil.com/support/docs/3215.htm

    in addition my KEIL Version is 3.04(This sequence is implemented in UL2ARM.DLL V1.20a or higher which is part of MDK-ARM Version 3.02.).It not help.

    And i tried to do just full erase -> i receive COULD NOT STOP ARM DEVICE.

    Is it means that i must to change the chip on the board ? Please somebody

    help me!!!!!!!!!!!!!!!! Pliiizzzzzzzzzzzzzzzzzzzzzzzz!!!!!!!!!!!!!!!

    k_arthurAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:40

    Ibtissem . I have read your detailed explanation of how to boot from bank1.

    In this part:

    The most important options are:

    - BBSIZE 0x32K

    - BBADDR 0x0

    - NBBSIZE 0x512K

    - NBBADDR 0x80000 (and NOT 0x400000!)

    - NBBADDR is not obligatory to be 0x80000

    Its better to set it -> 0x8000 (32 kb from 0x0) Am i right?

    Please check it and answer me. Simply I afraide of STR911.

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:40

    Keil ARM MDK 3.05 is now valid, may be, erasing a not responding

    device is is working only with this newer version, you can download mdk 3.05 from the Keil homepage.

    [ This message was edited by: Barricade on 28-03-2007 13:59 ]

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:40

    A second possibility is to use the ST tool CAPS with

    a ST flashlink adapter. Booth solutions worked for me.

    k_arthurAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:40

    Written on chip :

    ARM

    STR911F

    M44X6

    HPAEW VG

    KOR HP 620

    ST

    k_arthurAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:40

    Additional information:

    I work with boards developped by firm i work in. And we tried 2 boards

    and make the same mistake twise(forget to set bit CSX (may be because

    STR91xCFG.s was not added to new project)). The problem is exist on 2 boards. Both boards show the same response.

    k_arthurAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:40

    Hello ibtissem,

    thanks for help.

    Another question:

    BBADDR is obligatory to be 0x0 or it is possible to use another

    value in some situations? Simply i do not anderstand why we have

    opportunity to change BBADDR.

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:40

    I had the same problem twice. The first time I replaced the STR912 device :|

    The second time I bought me a RLINK device (raisonance). In combiantion with CAPS, I erased flash ! I was not able to do this with my ULINK .

    Luc Vercruysse