Skip to main content
Visitor II
February 25, 2005
Question

KWP2000 Protocol Implementation on ST7/ST9 ?

  • February 25, 2005
  • 7 replies
  • 2039 views
Posted on February 25, 2005 at 05:00

KWP2000 Protocol Implementation on ST7/ST9 ?

    This topic has been closed for replies.

    7 replies

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:33

    How to implement KWP2000 diagnostic protocol on a K-line Physical medium with ST7 or ST9 microcontroller ?

    Is it possible to perform both a 5-baud Initialisation (address code recovery) or a fast initialisation without

    inducing any error on a typical SCI peripheral ?

    Is there any reference application available ? (Work around using an additionnal I/O for address code detection ?

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:33

    What is KWP2000 ?

    Breizh

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:33

    KWP2000 stands for KeyWord Protocol 2000 : It' s based on the international standard ISO14230-4.

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:33

    The ''K'' line is basically a sci port with a non-standard baud rate.

    For instance, Dodge uses 7182 baud for ISO diagnostics.

    I know it has already been implemented on several ST92F150 applications but there isn't any reference design available.

    Good luck for your design

    Jojo

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:33

    Hy,

    The KW2000 protocol is related at Automotive sector.

    K line is a half duplex serial line that use a SCI hw cell.

    The application and diagnostic services are strongly defined by specification dedicated to the application.

    Then if you don't have these specification will be very hard implement sw.

    By
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:33

    Could U please elaborate more on KWP2000 protocol. I am going to work on it.

    :-[

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:33

    hi

    any idea on where i can find kwp2000 hardware schematics.