Skip to main content
Visitor II
February 20, 2024
Question

L6470

  • February 20, 2024
  • 0 replies
  • 1092 views

Hi,

I am using

a) L6470 to control Stepper motors. I am using STP-MTR-23079(x). The motor has rated current=2.8A/phase, Resisteance=1.1ohm/phase.

b) I am using 24VDC for L6470.

c) I am setting KVAL = 14.04% with phase current that is around 3.07A/phase.

 

Here are the problems I have:

1) When I run the motor with speed=30.5 steps/s, it works fine

2) When I run the motor with speed=247.9 steps/s, there is no enough torque.

3) I am trying to do BEMF compensation based on formula from DT00065 design tip:

Vp = [Vs (KVAL_RUN/256) + Vs(INT_SPEED/250)(ST_SLP/256)] + Vs(DELTA_SPEED/250)(FN_SLP_ACC/256)

KVALRUN=14.04, INT_SPEED=1032, ST_SLP=24, FN_SLP_ACC=40. I found the result is much high as what I want. Could you tell me if I did something wrong? How to do the compensation for higher speed?

Thanks,

 

Christie

    This topic has been closed for replies.