L6983N50QTR adjusting inductor and output caps
Hi,
Ive been trying to use eDesignSuite to verify my design with L6983N50QTR. Please find my schematic attached. My specs are:
IC
L6983N50QTR
Topology
buck
Input
7 - 33 V
Output 1
5 V (2 % ripple) - 1.9 A max
When I put the values that I am trying to use, I get the warning that the IL ripple is 30.27%, and bandwidth is 18.29kHz. In my schematic I adjusted the inductor to 10uH and added more output capacitors but how do I do it on eDesignSuite? I tried to change inductor value but it doesnt work. Could you please check this circuit and let me know if this is ok? Thanks