Question
L99LD21Q6TR Led driver IC (What to know its best Switching Frequency)
Hi,
L99LD21Q6TR is a LED driver (Buck and Boost).
For my application, i am using Boost separate and Buck separately. This IC Frequency range is 100KHz to 450KHz.
My design consideration for Boost is
- Input voltage range: 10 V to 16 V
- Output voltage: VBOOST: 35 V
- LED current or Output current: 450 mA
My design consideration for BUCK is
- Input voltage: VBUCKIN: 14 V
- Output voltage: VLED: 10.1 V
- LED current or Output current: 1.4 A
what is best frequency for Boost and what is best frequency for Buck?