last 3 bytes not written to eeprom page during page write
Hi,
I have a weird issue !
I am developing an application where i Use the M24C64-WDW6TP EEPROM.
First I need to be sure, this eeprom have 8KB of memory, every page is 32B so it has 256 pages.
is the page address = (page number - 1 )*page_size ?? for example when I want to write to the second page, the address has to be 32 = 0x0020?
If I want to write to the second byte in the second page this byte address is 0x0021?
Second I have an issue where I try to write 32 bytes to a page,
The issue is that the lat 3 - 4 bytes is not written to the eeprom and I noticing that when I read the same page after I write it.
Do someone recognize this problem !?
Please help
Best Regards
Jawad