Skip to main content
Visitor II
February 19, 2004
Question

LCD Enable Timing

  • February 19, 2004
  • 3 replies
  • 704 views
Posted on February 19, 2004 at 20:43

LCD Enable Timing

    This topic has been closed for replies.

    3 replies

    sjoAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:58

    I have just noticed the timings used for the LCD (DK3200/DK3300) dev boards are not within spec for a typical intelligent lcd.

    The main point I have noticed is the enable line, this is set for approx 130-140ns (@36MHz) this should be minimum 230ns (total cycle 450ns) to comply with the Hitachi spec.

    Surely if the dk boards are used as a design starter, they should comply with these timings ?

    Regards

    sjo
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:58

    Thanks for your input, we will look into it. By the way, the LCD used on the DK boards are Hantronix not Hitachi.

    sjoAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:58

    Thanks for your reply.

    I was really referring to the chipset, as nearly all (Samsung,Novatek,Sitronix,JRC) are based on the Hitachi HD44780 controller, even though Hitachi have stopped making this.

    Regards

    sjo