Skip to main content
Visitor II
January 7, 2004
Question

LCD module

  • January 7, 2004
  • 3 replies
  • 1019 views
Posted on January 07, 2004 at 12:08

LCD module

    This topic has been closed for replies.

    3 replies

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:57

    I am designing an application based around the uPSD3234BV-24U6. I need a 2 x 16 LCD display which is compatible with the 3.3V operating voltage of the uP. The LCD module can use a 5V supply, but must have 3.3V compatibility. If anyone can supply me with the reference of a suitable display I would most grateful.

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:57

    Yes, but I'm not sure of full compatibility.

    The uPSD3234BV operates voltage is 3V3 and the HDM16216H operates voltage is 5V.

    I have connected the LCD to the port A of the µP, like DK3200 eval board, but port A of the µP is not tolerent to 5V

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:57

    How about the Hantronix HDM16216H-B-P93S which is used on the DK3200 eval board? I think their contact number is (40 517-4