LED1202 Script Execution is Impossible
Hello,
So it seems like the software package X-CUBE-LED12A1, which is essentially a basic C driver for (some) of the dev kits, contains no support for uploading, downloading, starting or stopping execution of scripts. The commands are present in bridge.h, but not actually implemented in what looks to be an old release of the software.
uBasic scripts is one of the advertised features of the LED1202, and you can do it through the windows application and the closed source binary firmware for the L0/L4/F4 found here.
I have no proof, but it appears the scripts are converted into i2c commands on the STM32.
Can someone at ST update the latest source: https://www.st.com/en/embedded-software/x-cube-led12a1.html#st-get-software or provide a link to source in https://www.st.com/en/evaluation-tools/steval-lll007v1.html#tools-software
Without the source, I cannot use the uBasic functionality on the project.