Skip to main content
Visitor II
July 11, 2017
Question

LM339 input voltage

  • July 11, 2017
  • 0 replies
  • 530 views
Posted on July 11, 2017 at 12:56

As per data sheet of LM339, the input voltage range is from -0.3V to 36V. We are using LM339 as a Comparator in our circuit , in certain cases, we have a voltage of -0.7V at Vin ( inverting). which is above the specification. Will it cause damage to Opam? What will be the behavior of Opam in this case? VCC is +24V and GND.

    This topic has been closed for replies.