Did anybody successfully load WinCE.net or early version of WinCE to atlas board? We did it, bit network card driver doesn’t work and the mouse can’t work either. Please give me some guide. Thank you very much!
I have managed to upload an image through the network reliably using an ISA board called Linksys.
It is possible to use PCI based cards and I managed to use a Realtek 8139 but you have to disable to wrtie posting and read prefetch options in the BIOS beforehand.
We use the STPC with Intel 82559ER chip. There are two drivers out there. First one from Intel itself to which works fine on WinCE 4.x and one from FS Force on Platform Builder 3rd Party CD to support Kernel Debugging over Ethernet on Intel chip. Both work fine on our hardware.