I am using RVDK 2.1. When I compile my project and try to load the new image into RAM when there is already an image loaded i get an error like this: Existing image '' has addresses that overlap with the 'RAM' section Failed loading 'C:\Documents and Settings\ewitt\My Documents\p2d\ARM7filez\myproject\backup\example2\Debug\Example2.axf' I did not have the problem before. Now i am getting this error every time. The only solution is to deconnect the debugger, turn of the ARM connect again and then load the image. any suggestions? cheers, Erwin