Skip to main content
Visitor II
February 26, 2005
Question

Locating absolute segment (program/constants) using the STVD7 3.0

  • February 26, 2005
  • 2 replies
  • 693 views
Posted on February 26, 2005 at 08:00

Locating absolute segment (program/constants) using the STVD7 3.0

    This topic has been closed for replies.

    2 replies

    Visitor II
    February 25, 2005
    Posted on February 25, 2005 at 20:28

    Using the STVD7 3.xx we tried to locate an absolute segment at sector 1 of 72F521N9 with no success.

    Using STVD7 2.54 this was done with the following command:

    # locate .e4dTP1 at -b0xe000

    +seg .e4dTP1 -b0xe000 -n .e4dTP -m4096

    d:\sw\e4Gen\object\T4cons.o

    How can I do that using STVD7 3.xx? Any syggestions anyone?

    Visitor II
    February 26, 2005
    Posted on February 26, 2005 at 08:00

    similar method, you need to overide the generated linker script via project settings/linker input and uncheck the auto checkbox.

    modify script as you did in the older version.

    Regards

    sjo