M24C01/M24C02 device addressing restriction
Hi,
We're developing a PCB that can have multiple different I2C ICs assembled and have chosen the M24C02-RMC6TG EEPROM for board identification.
In the datasheet, section 4.5, a note states no other device using the 1010 xxxx address can be connected to the same bus. The note also begins with "When using the DFN5 package:".
I'm unsure whether this statement applies only for the DFN5 package or in general? (Datasheet snippet below)

One of the intended ICs that we plan to implement can be configured to have either 1010 011 or 1010 010 I2C address. Can this IC be on the same bus with this EEPROM? (With the address configured to not overlap with the other IC)
Thanks in advance,
Lazar