Skip to main content
Visitor II
November 8, 2004
Question

MCO clock problem in ST7liteS2

  • November 8, 2004
  • 3 replies
  • 870 views
Posted on November 08, 2004 at 09:19

MCO clock problem in ST7liteS2

    This topic has been closed for replies.

    3 replies

    moshe_eAuthor
    Visitor II
    November 8, 2004
    Posted on November 08, 2004 at 05:04

    Hello All,

    I encountered a difficulty to use the MCO function.

    I set the option bytes to RC oscilator, PLL ON, PLLX8 and set the MCO bit in the MCCSR (MCCSR |= 0x02

    , BUT no clock is out!!!

    Please Advise.....

    Thanks in advance

    Visitor II
    November 8, 2004
    Posted on November 08, 2004 at 08:30

    Hi Moshealb,

    if you do define the port PA6 neither as output with push pull nor as open collector with external pullup you might get this problem.

    I didn't try it but think it can be the reason.

    Best regards, WoRo
    moshe_eAuthor
    Visitor II
    November 8, 2004
    Posted on November 08, 2004 at 09:19

    Dear WoRo,

    the advice was helpfull, but now I encountered another problem:

    the board is working with the inDart connected but when I leave the Metrowerks enviroment and Power up, the MCU stop working.

    the option bytes are defined as follow:

    -write protection = off

    -read-out protection = off

    -sector 0 = 1K

    -No reset in halt

    -watchdog = software

    -LVD = OFF (with Power up Reset device + Open collector +pullup)

    (I also tried ''LVD = lowest voltage'' with no Reset device)

    -RC Osc. = ON

    -PLL = Enabled

    -PLL X8

    what could possiably be the resone for this problem?

    Thanks Again....