Skip to main content
Visitor II
September 24, 2023
Question

MCU Selection - SD24 + Load Cell

  • September 24, 2023
  • 2 replies
  • 1003 views

I need help with MCU Selection.

The main aim is to replace (STM8s and HX711) Chips in a weight scale project.

So, the MCU should be low in cost, include an SD24 with PGA Gain 128.
It also should include SPI interface.

Note: Load cell maximum weight could be greater than 200kg.

    This topic has been closed for replies.

    2 replies

    Graduate II
    September 24, 2023

    Hello @Sadeen 

    Can you explain more about what exactly you want to do .

    Best regards.

    II

    Graduate II
    September 24, 2023

    None of the STM32's have a 24-bit Sigma-Delta. Pretty much every one of the STM32 has multiple SPI buses, or could bit bang one.

    Perhaps you can expand on why the current implementation isn't working, and what other features newer parts would add to the final project? Computer connectivity? LCD / User Interface?

    MSP430AFE2x3 has a "SD24"