MEMS Board and accelerometer

I have finally isolated an example of the error. The MKI 210 accelerometer + the test board is sitting attached to a NUC computer. The entire setup has run for months with no problems at a REMOTE LOCATION that is very hard to get to without a lot of effort.
Using the software I wrote from your base program in C#, the program is telling me it cannot connect to the accelerometer.
I rebooted the computer over the net and it still gives the same errors.
Now I have trapped one, I downloaded UNICO-GUI to the computer and then ran the program and got the following error. I checked on one of the accelerometers in my lab and it worked perfectly.
THE ONLY WAY I CAN GET THIS ACCELEROMETER TO WORK IS TO COMPLETELY DISCONNECT THE USB CABLE FROM THE COMPUTER AND LET IT DIE FOR A MINUTE. THERE ARE NO OTHER TESTS I CAN PERFORM -
I do not want to drive a long distance to plug and unplug a cable.
Is there a command I can send the board to do the same thing and overcome the error seen above.
It was working perfectly yesterday as are the other ten devices that are identical.
I have raised this issue before, but your advice would be appreciated as I never got a reply that worked
John