We are using Micrium's TCP/IP stack and are having a problem. Scenario: * Code running on an IAR STR912 dev board which is connected to LAN through the ethernet connector. * Code compiled using IAR tools * PC, also on lan, used to ping IAR board. * ICMP Ping replies come up in < 1ms * ICMP Ping reply * If connected to large LAN with broadcasts, Ping response time suddenly starts to exceed 1ms after a while....builds up higher and higher to be over a second....and then after a while, the whole MCU freezes. Has anyone else seen this? Any help will be appreciated! Thanks Nirosh
well, to debug your TCP/IP problem, you need a packet sniffer -> your best friend is : Ethereal, now the name is WireShark. Just plug a Hub (WARNING : it's not a switch) between your network and your STR912 board. Connect ot this hub your Pc with Etheral and you will be able to look all frame. If you use a switch, you will only look multicast and broadcast frame, it's not accurate but could be a good beginning for a 1st try. Best regards. Damien