Need a datasheet for a IC (8 pins) of Power Suply Inverter (Motorolla charger)
I got a Motorolla Charger (PSM4604A):

This is the circuit:



This adapter gives 4.2 V but i need a 5.2 V to charge my smartphone, so i have to rise this constant voltage. But here is a problem. On cold part of circuit there are 3 IC that doing something including voltage control. One of them with 6 pins. But other two, with 8 pins, are relative to each other. This one:

And this one:


This two Chip made by STMicro - B941 & B942 are sort of comparators maybe, or amplifiers. The one that lays on own vertical miniboard does the job of current protection(B941). The other lays on main motherboard(B942) doing Voltage Control. But I couldn't find datasheet of it. I think this mark B942 is not full, gotta have some other codes that helps to search datasheet. So if anybody can help please respond. Thanks in advance.