Skip to main content
Visitor II
November 7, 2008
Question

need help for CAN Configuration !

  • November 7, 2008
  • 1 reply
  • 595 views
Posted on November 07, 2008 at 07:18

need help for CAN Configuration !

    This topic has been closed for replies.

    1 reply

    nr_naikAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:56

    I want to run the CAN @ 1Mbps for PCLK of 48MHz. Need help for settings of the can bit rate settings.

    I tried 1Mbps @8MHz Pclk ( which is available in the CAN library function ) , that works fine.

    Now using the calculation information the settings for 1Mbps with 48MHz PCLK , comes out to be Time QUANTA = 8, Tseg1 = 4, Tseg2 = 3, BRP = 6 & SJW = 1 to 4. But this setting does not work.

    NEED Help for this settings.

    Need these settings and guidance for calculations.