Skip to main content
Visitor II
May 30, 2016
Question

Newbie STR710 prgm s/w tools?

  • May 30, 2016
  • 1 reply
  • 681 views
Posted on May 30, 2016 at 09:06

Hi All, 

 First, I am completely new to ST Micro devices.

  My experience is with microchip/atmel.

It is my hope that by joining & posting on this forum,

 I can learn and grow with this procc family.

 I recently received a PCB populated with a STR710FZ2T6 device

The PCB has some i/o eg leds and switches onboard, type of a eval board I guess.

 Well, I would in fact like to use it to eval this proc.

Onboard is also a RS232 port (TX/RX only),

  connected to Pin1 (P0.11) and Pin2 (P0.10)

I know that it is working because on Power-On, I receive a

sign-on msg 'Connected' and when I press spacebar, response is '!'

  Comms params 4800/8/n/1

On Power-up I observe that 2 leds blink alt on/off.  So I assume the brd is functional.

I would like to know if there is windows s/w available to prgrm the procc,

  with my future test code, via the existing RS232, like having  boot-loader onboard?

If the existing RS232-port cannot be used for programming the device,

 which port/configuration and s/w tool is std to be used to prgm the device?

   Recommended circuit for prgm and the required s/w prgm module?

There is proto space available on the brd, so I can solder on comp/conn

to make-up a prgm port interface.

At this time I don't want to buy a prgmer/debugger/sw for my inital eval, until

I can at least get a led to blink  with my code. ~)

 Therefore, I am  hoping that there is a 'freeware/public domain' prgm sw tool available?

Any pointers or advise will be appreciated.

Thank you.

Gerhard

#gg-str7
    This topic has been closed for replies.

    1 reply

    Graduate II
    June 21, 2016
    Posted on June 21, 2016 at 03:44

    The part is extremely obsolete at this point  (ARM7 2005)

    http://www.st.com/content/ccc/resource/technical/document/datasheet/b1/05/dc/08/6d/13/46/66/CD17652091.pdf/files/CD17652091.pdf/jcr:content/translations/en.CD17652091.pdf

    As I recall you're going to have to program it initially via JTAG (ie J-Link or U-Link)

    Might I suggest something in the Cortex-Mx family on a NUCLEO or DISCO board