Skip to main content
Visitor II
December 23, 2005
Question

_nop_()

  • December 23, 2005
  • 3 replies
  • 1049 views
Posted on December 23, 2005 at 12:44

_nop_()

    This topic has been closed for replies.

    3 replies

    jmAuthor
    Visitor II
    December 20, 2005
    Posted on December 20, 2005 at 13:02

    Hi,

    I have just taken a project already started on the ST10F168. My problem is to understand when I am obliged to use the _nop_() function. Because in my project, it's using in abundance...Is it really necessary ??

    When you set a port or a state(input/output), do you put a _nop_() (or 2) after ??

    In general, when the use of this function is necessary ??

    Thanks in advance

    Regards

    JM

    jmAuthor
    Visitor II
    December 21, 2005
    Posted on December 21, 2005 at 10:27

    Thanks

    So, NOP are necessary just after changing the state of one port pin direction of a port, or also after changing the value of the port pin ?

    which NOP are necessary in the example below. Just 1 (or 2) after changing the direction, or all ?

    Code:

    P8=0xFF;

    _nop_();_nop_();

    DP8=0xFF;

    _nop_();_nop_();

    Regards

    JM

    jmAuthor
    Visitor II
    December 23, 2005
    Posted on December 23, 2005 at 12:44

    Thanks again !!!!