Skip to main content
Visitor II
April 20, 2007
Question

OFDM over str9

  • April 20, 2007
  • 2 replies
  • 993 views
Posted on April 20, 2007 at 12:23

OFDM over str9

    This topic has been closed for replies.

    2 replies

    gabriele2Author
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:39

    I would like to know if some one have try to implements an OFDM modulation using for examples an STR9. I see that it can perform an 256Point FTT in about 200us.

    I see also that this device have an 10Bits A2D with a convertion time of 1uS.Is possible in some way to increase the ''sensibility'' form 10bits to 12Bits?

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:39

    Actually, I've got the same problem. I'd like to control a robot using WLAN ieee 802.11 b. I know I have to modulate somehow signal from MAC unit though I don't know signal parameters. I would appreciate the answer if there's on the market any baseband processor (for OFDM modulation and signal conditioning) so that I could easily connect my STR912 to such baseband processor and then to ZIF transceiver.Are there such devices on the market? If not then how to enable STR912 to communicate through WLAN - (WiFi)?