I been banging away at this all day, help me out here while I still have some hair left. I have read that you would like the code posted so some comment can be made on it. OK, just remember that you asked. The routine sticks at C2_LP, it never sees the TI in SCON2 for the second UART IICSDA is a diag pin (P3.1) that I use to track stuck routines. The transmit routine uses “RSDAT�? as a charter buffer in the ram to load the sbuf2. ********************************************************** C2_OUT: mov A,IEA clr Acc.4 ;Clear the second UART Interrupt enable mov IEA,A mov SBUF2,RSDAT C2_LP: mov A,SCON2 cpl IICSDA jnb Acc.1,C2_LP clr Acc.1 mov SCON2,A mov A,IEA setb Acc.4 ;Enable the Interrupt enable mov IEA,A ret And the setup routine for all the timers, and “stuff�? Just remember you asked ! ;****************************************************************** ;* Timers 0 thru 2 set up ;* Timer 0 ....... tclk ;* Timer 1 ....... RS232 Port 0 ;* Timer 2 ....... UART1 ;****************************************************************** S_INT: clr TR1 mov TMOD,00100001B ;Timer 1 is set to 8 bit auto reload mode ;Timer 0 used as 16 bit Tic clock ;Reload the tic value on interrupt mov th1,BaudLoad ; Set reload value setb tr1 ; start timer for UART 0. ;****************************************************************** ;* TCON * ;* bit0 IT0 External Interrupt 0 type H/L state * ;* bit1 IE0 External Interrupt 0 flag * ;* bit2 IT1 External Interrupt 0 type H/L state * ;* bit3 IE1 External Interrupt 0 flag * ;* bit4 TR0 Timer 0 run flag * ;* bit5 TF0 Timer 0 overflow flag * ;* bit6 TR1 Timer 1 run flag * ;* bit7 TF1 Timer 1 overflow flag * ;****************************************************************** mov TCON,01010000B ;Start both timers ;****************************************************************** ;* Timer 0 setup and run * ;****************************************************************** mov tl0,ticl ; Set reload value mov th0,tich ; Set reload value setb tr0 ; start timer 0. setb et0 ; set the interrupt enable ;****************************************************************** ;* Second UART setup and run * ;****************************************************************** ;* PCON * ;* bit0 IDL Active Idle Mode high enable * ;* bit1 PD Power Down high enabled * ;* bit2 TCLK1 Transmit clock flag UART2 * ;* bit3 RCLK1 Receive clock flag UART2 * ;* bit4 ADSFINT Enable ADC Interrupt * ;* bit5 LVREN LVR Disable bit active high * ;* bit6 SMOD1 Double baud rate UART2 * ;* bit7 SMOD Double baud rate UART1 * ;****************************************************************** ;* SCON / SCON2 * ;* bit0 RI Receive Interrupt Flag * ;* bit1 TI Transmit Interrupt Flag * ;* bit2 RB8 8th bit received * ;* bit3 TB8 8th bit transmitted * ;* bit4 REN Enable Serial reception, * ;* bit5 SM2 Multi uP addressing enabled * ;* bit6 SM1 UART type used with SM0 * ;* bit7 SM0 UART type used with SM1 * ;****************************************************************** ;* SM1 & SM0 S/B ''10'', in binary * ;* SM2 low to disable the multi processor function * ;* REN set to enable port * ;* ignore the 8th bit flags * ;* TI / RI are reset by the IRQ handler * ;****************************************************************** ;* Second Interrupt Enable IEA * ;* IEA * ;* bit0 EUSB Enable USB Bus * ;* bit1 EI2C Enable IIC Bus * ;* bit2 NU Not Used * ;* bit3 NU Not Used * ;* bit4 ES2 Enable 2nd Serial reception * ;* bit5 NU Not Used * ;* bit6 NU Not Used * ;* bit7 EDDC Enable DDC Interrupt * ;****************************************************************** MOV SCON, 050h ; Timer 1 : Mode 1 (vari baud) ; and set receive enable MOV SCON2, 050h ; Timer 2 : Mode 1 (vari baud) ; and set receive enable SETB TR1 ; Start timer 1 ;mov SCON,01010000B ;TI set indicates transmitter ready. ;mov SCON2,01010000B ;TI set indicates transmitter ready. ;mov A,PCON ;setb Acc.2 ;setb Acc.3 ;mov PCON,A ;Set the uart to run from timer 2 mov PCON,00001100B ;Set the uart to run from timer 2 ;mov PCON,00000000B ;Set the uart to run from timer 2 mov TL2,SECUART ; Set reload value mov TH2,SECUART ; Set reload value mov RCAP2L,SECUART mov RCAP2H,SECUART ;Load the 16 bit counter with reload value mov IEA,00010000B ;Set the 2nd uart interrupt enable ;mov T2CON,00000100b ;mov T2CON,00110100b mov T2CON,030h ret
It winds up to be that you can’t use timer 2 with uart 1, when you have both uart1 and uart0 on separate timers.
In other words, when using two uarts, at separate baud rates, timer 1 must go to uart 1, and timer2 must go to uart 0. I found this answer in one of the st documents, but I now forget which. Good to see the forums are still alive. Many thanks all.
It's a pity you don't remember where did you read about it...
By the way, I am using Timer2 for UART1 and Timer1 for UART0 and both are working... Maybe there is a difference in the chips? Mine is uPSD3212C Jan Waclawek
On 22-05-2006 at 11:15, Anonymous wrote: It's a pity you don't remember where did you read about it... By the way, I am using Timer2 for UART1 and Timer1 for UART0 and both are working... Maybe there is a difference in the chips? Mine is uPSD3212C Jan Waclawek There is a difference in the chips, I got the 3254a in an 80 pin package. The notice was in one of ST's quality reports, so I switched timers, and everything worked.