If i set the interrupt sensitivity as ''rising edge & high level'' then in that case the time for which the level on the interrupt pin should be high(i.e. pulse width) is 1tcpu for an interrupt to be detected but my question is when does a processor keep it in the list of pending interrupt. Is there any time for which if the level remains high ,processor keep it into the list of pending interrupt .
in fact, when setting an interrupt sensitivity as ''rising edge and high level'', an interrupt will occur when a high level occurs (IRQ line set) and it's when the it routine address is fetched (present on the address bus) that the IRQ line goes low, but if during this time, your signal applied on the ext I/O is still high, then an interrupt request will once again occur (IRQ line goes high) and the same interrupt will be pending. If you don't want to have several interrupts, you can select ''rising edge only'' sensitivity, otherwise it's up to you to manage your interrupt signal . [ This message was edited by: stef on 12-02-2003 10:54 ]
you have said that it checks for the HIGH level before going into the main routine. Is it like just before executing IRET instruction...... Thanks for the answer [ This message was edited by: Ranjeet on 14-02-2003 06:09 ]