Skip to main content
Visitor II
August 21, 2025
Solved

PLC module with ADC and mcu

  • August 21, 2025
  • 1 reply
  • 841 views

Could you please suggest a PLC module that includes a signal scaling unit and an isolation circuit, equipped with a high-speed sampling ADC with up to 16-bit resolution? The module should also integrate a microcontroller featuring SPI, LAN (Ethernet), SD card storage, and an HDMI port.”

    This topic has been closed for replies.
    Best answer by Peter BENSCH

    Welcome @rakesh1184, to the community!

    What do you mean by PLC – Power Line Communication or a Programmable Logic Controller?

    In both cases, however, STMicroelectronics does not offer ready-made modules. For these, you will need to contact the relevant manufacturers.

    Regards
    /Peter

    1 reply

    Technical Moderator
    August 21, 2025

    Welcome @rakesh1184, to the community!

    What do you mean by PLC – Power Line Communication or a Programmable Logic Controller?

    In both cases, however, STMicroelectronics does not offer ready-made modules. For these, you will need to contact the relevant manufacturers.

    Regards
    /Peter