I need to get my St7 Lite on power saving mode (only battery) but I need to wake up sometimes (0.5-1s) to check my probes. - Is possible to do? - If yes, How I can wake up my micro? with external interrupt (needs more component??)? or internal interrupt ?? Is there any Application Note ? Many tanks in advantage!! MBKS
ST7FLITE1x and ST7FLITE2x have an internal oscillator that can be used to wake-up the micro when it is in HALT mode. For ST7FLITE0x and ST7FLITESx, the AN1605 explains how to wake-up the micro by an external RC circuit. Regards, EtaPhi