Skip to main content
Visitor II
June 29, 2009
Question

Problem ICP programming ST72F324L device with STVP

  • June 29, 2009
  • 2 replies
  • 815 views
Posted on June 29, 2009 at 14:43

Problem ICP programming ST72F324L device with STVP

    This topic has been closed for replies.

    2 replies

    patm4Author
    Visitor II
    June 29, 2009
    Posted on June 29, 2009 at 14:43

    I have been developing an application on the ST72F324LK6T6 with DVP3.

    During emulation all is well.

    When I solder chip to app board and try to ICP program (with STVP ) I get an error message ''PROBLEM DOWNLOADING MONITOR''

    I have programmed many devices with this setup and not had problem, but this is the first time on the 3v parts.

    I have done the following:-

    1) Checked the ICC schematic against the datasheet.

    2) Removed target crystal, connected ICCOSC to OSC1 and connected OSC2 to GND. The ICCOSC signal has been checked with a scope for the presence of a clock.

    3) Checked DVP settings ICP-OPT Disable and 3V app. supply switch setting.

    I have read a little about the ICC protocol and have confirmed the pulses on ICCDATA.

    One thing I did note was that the VOH levels on the ICCDATA and ICCCLK are a little marginal ( 2.4-2.5v ). I tried pullup resistors on the app board on these lines but it made no difference.

    The RESET and ISPSEL lines also seem ok.

    Any suggestions ?

    Are there any firmware updates for DVP3 ?

    Visitor II
    July 29, 2010
    Posted on July 29, 2010 at 07:31

    .ExternalClass23B559A9A8F945A4B8214D961234490B p.MsoNormal, .ExternalClass23B559A9A8F945A4B8214D961234490B li.MsoNormal, .ExternalClass23B559A9A8F945A4B8214D961234490B div.MsoNormal {margin:0in;margin-bottom:.0001pt;font-size:11.0pt;font-family:'Calibri','sans-serif';} .ExternalClass23B559A9A8F945A4B8214D961234490B .MsoChpDefault {font-size:10.0pt;} @page Section1 {size:8.5in 11.0in;margin:1.0in 1.0in 1.0in 1.0in;} .ExternalClass23B559A9A8F945A4B8214D961234490B div.Section1 {page:Section1;} Did You Get Solution for this.

    Kindly Share if You have.