Skip to main content
Visitor II
October 20, 2004
Question

Problem in Programming uPSD3254A

  • October 20, 2004
  • 2 replies
  • 645 views
Posted on October 20, 2004 at 14:48

Problem in Programming uPSD3254A

    This topic has been closed for replies.

    2 replies

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:03

    Hi,

    I am using RLink cable for programming uPSD3254A with PSDsoft Express. When I installed RLink driver, the PSDsoft Express provides me only one option while programming (Full chip program) and all other options (flash only...) are disabled. So I am doing a full chip programming each time. Is there any way to program only the flash. Its urgent can anybody suggest me a method to program only the flash.
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:03

    You can use the Ride software to program the uPSD32xx family of products. There is a programming option for just the flash. The Ride software is on the CD that was in the box with RLINK-ST. AN48 (also on the CD) explains how to program a uPSD32xx device. If you have further quesitons, please contact the applications engineering department at:

    mailto:apps.psd@st.com

    .

    Also, in order to better serve you, please provide the following information:

    Name

    Company Name

    Phone Number

    Location (City, State, Country)

    Production PSD/uPSD part number (81x, 91x, 32xx, 33xx, etc.)

    Microcontroller/Microprocessor

    Application

    Projected annual volume (units)

    Production start date

    PSDsoft Express version