Skip to main content
Visitor II
May 27, 2003
Question

Problem to start framebuffer

  • May 27, 2003
  • 2 replies
  • 863 views
Posted on May 27, 2003 at 13:41

Problem to start framebuffer

    This topic has been closed for replies.

    2 replies

    galAuthor
    Visitor II
    May 27, 2003
    Posted on May 27, 2003 at 11:52

    Hello,

    I test my new kernel with:

    1.General Software BIOS+LILO

    2.Phoenix BIOS+LILO

    This is the same kernel I used with stpc loader.

    I have the following result:

    1.with the General Software BIOS after I chose the operating

    system from the LILO menu the system restart automatically.

    In the lilo.conf file I added vga=ask (and install the new loader by

    running the lilo command in the terminal window) but it has

    the same affect.

    2.With the Phoenix BIOS the system is also restart automatically but

    when I added vga=ask in the lilo.conf file and restart the

    computer I chose the new resolution and the linux didn’t continue

    to load. It beeps 8 times and the POST code show 22.

    I attach the new kernel I created.

    What do you advice me to do?

    Thanks in advance.

    Visitor II
    May 27, 2003
    Posted on May 27, 2003 at 13:41

    With a solution BIOS+LILO, you must use the bzImage version of the kernel you get in usr/src/linux/arch/i386/boot after a 'make bzImage'. It is not exactly the same as the vmlinux you get from usr/src/linux.

    Even if the frame buffer device is not well installed, your kernel should work at least in text mode.

    Farfalla