Skip to main content
Visitor II
April 22, 2004
Question

Problem with ADC using ST72F324J2

  • April 22, 2004
  • 4 replies
  • 1011 views
Posted on April 22, 2004 at 07:17

Problem with ADC using ST72F324J2

    This topic has been closed for replies.

    4 replies

    fred2Author
    Visitor II
    April 21, 2004
    Posted on April 21, 2004 at 09:41

    Hi!

    I have just started to use the Metrowerks CodeWarrior C compiler and have a problem with the A/D CONVERTER.

    I want to use the AIN2, AIN3, AIN4, AIN5. (PD2 to PD5 ST72F324J2)

    When i use only one channel, All is ok.

    But when i want to make the acquisition of one channel after one channel, it's not ok.

    I have a function that is named Adc()

    void Adc(void)

    {

    ADCCSR = 0x22; // Channel 2

    while (!(ADCCSR & 0x07));

    In_ana2 = ADCDRH;

    ADCCSR = 0x23; // Channel 3

    while (!(ADCCSR & 0x07));

    In_ana3 = ADCDRH;

    ADCCSR = 0x24;

    and so

    ...

    }

    If i use only anyone channel the acquisiton in the variable In_anaX is correct.

    But if use all the channel, the acqusition in the variable is false.

    What is my mistake?

    /Fred.B

    Visitor II
    April 21, 2004
    Posted on April 21, 2004 at 14:02

    For checking the End of conversion you have to use

    while (!(ADCCSR & 0x80));

    But you are using ''while (!(ADCCSR & 0x07));''.

    You can also download the ST7 software library to have the ''ADC code'' from the same site.

    fred2Author
    Visitor II
    April 21, 2004
    Posted on April 21, 2004 at 14:43

    Hello,

    Thanks Jatin.

    Could you give me the links to the ST7 software library because i have found in this site the AN979 but in this apllication note there is only the main code and it refers to the library. Example ADC_Enable();. The problem was the link :http://cmg.st.com/stonline/products/cmg/mcd/st7.html (ST7 software library version1.1). It doesn't match.

    So could you give me the right link to download the ST7 software library included ADC_Enable() for the ST72F324

    Fred.B

    Visitor II
    April 22, 2004
    Posted on April 22, 2004 at 07:17

    In the Main Menu Click - Downloads -> St7Microcontrollers -> Software-Microcontrollers->ST7 Software Library