Skip to main content
Visitor II
April 19, 2006
Question

problem with FLASH_WordWrite

  • April 19, 2006
  • 2 replies
  • 854 views
Posted on April 19, 2006 at 10:47

problem with FLASH_WordWrite

    This topic has been closed for replies.

    2 replies

    Visitor II
    April 12, 2006
    Posted on April 12, 2006 at 15:32

    Hello,

    this is an IAP with download via USB. It works fine, when I debug it, but when it runs normally, it seems to be disturbed by an IRQ, because the LR-Register is overwritten. The consequence is that it branches to nirvana. It seems to occure in FLASH_WordWrite().

    Best regards,

    Moe

    ________________

    Attachments :

    FW_L000100_WaMa_Download.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtNI&d=%2Fa%2F0X0000000aP8%2FB.Kier2abUDlvnsY0fWku5HjnJaJi8c8jFmxdElXbTA&asPdf=false
    Visitor II
    April 18, 2006
    Posted on April 18, 2006 at 06:56

    Hi,

    the frequency shouldn't be the problem. It's set to 8MHz. I don't read from flash, while I'm writing it. I use remapping to copy the flash program to the ram, to run the program from the ram.

    Thanks,

    Moe

    [ This message was edited by: Moe on 18-04-2006 11:39 ]