Skip to main content
Visitor II
December 26, 2007
Question

Problem with SSP0 reception

  • December 26, 2007
  • 6 replies
  • 1362 views
Posted on December 26, 2007 at 10:14

Problem with SSP0 reception

    This topic has been closed for replies.

    6 replies

    arnaudAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:45

    Hello,

    I have to drive a AT45D161 flash with the SSP0. The command sent by the SSP0 is correct and the AT45D161 responses datas to the SSP0 receiver. But the datas read in the STR9, stay at 0. Anyone has an idea ?

    N.B: In loopback mode the datas read are correct (datas sent).

    Here is my code.

    SSP0 Initialization :

    // P2.4 = CLK bus SPI

    GPIO_StructInit (&GPIO_InitStructure);

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;

    GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput;

    GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull;

    GPIO_InitStructure.GPIO_IPConnected = GPIO_IPConnected_Enable;

    GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt2;

    GPIO_Init (GPIO2,&GPIO_InitStructure);

    // P2.5 = MOSI bus SPI

    GPIO_StructInit (&GPIO_InitStructure);

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5;

    GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput;

    GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull;

    GPIO_InitStructure.GPIO_IPConnected = GPIO_IPConnected_Enable;

    GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt2;

    GPIO_Init (GPIO2,&GPIO_InitStructure);

    // P2.6 : MISO bus SPI

    GPIO_StructInit (&GPIO_InitStructure);

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6;

    GPIO_InitStructure.GPIO_Direction = GPIO_PinInput;

    GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull;

    GPIO_InitStructure.GPIO_IPConnected = GPIO_IPConnected_Enable;

    GPIO_InitStructure.GPIO_Alternate = GPIO_InputAlt1;

    GPIO_Init (GPIO2,&GPIO_InitStructure);

    // SSP0 Init

    SSP_StructInit(&SSP_InitStructure);

    SSP_InitStructure.SSP_FrameFormat = SSP_FrameFormat_Motorola;

    SSP_InitStructure.SSP_Mode = SSP_Mode_Master;

    SSP_InitStructure.SSP_CPOL = SSP_CPOL_Low;

    SSP_InitStructure.SSP_CPHA = SSP_CPHA_1Edge;

    SSP_InitStructure.SSP_DataSize = SSP_DataSize_8b;

    SSP_InitStructure.SSP_SlaveOutput = SSP_SlaveOutput_Disable;

    SSP_InitStructure.SSP_ClockRate = 0;

    SSP_InitStructure.SSP_ClockPrescaler = 2;

    SSP_Init(SSP0, &SSP_InitStructure);

    SSP_LoopBackConfig (SSP0,DISABLE);

    SSP_Cmd(SSP0,ENABLE);

    Datas Read :

    // send dummy byte

    SSP_SendData(SSP0,0);

    while(SSP_GetFlagStatus(SSP0,SSP_FLAG_TxFifoEmpty) == RESET);

    // read byte

    while(SSP_GetFlagStatus(SSP0,SSP_FLAG_RxFifoNotEmpty) == RESET);

    data = SSP_ReceiveData(SSP0);

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:45

    Hello arno,

    You should replace GPIO_IPConnected_Enable by GPIO_IPConnected_Disable,in P2.4 and P2.5 configuration.

    Please let me know if the problem persists.

    Best regards,

    mirou

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:45

    You should replace GPIO_IPConnected_Enable by GPIO_IPConnected_Disable

    What does the IP stands for? I found no explanation of it in the documentation.

    Would you please explain it?

    Thank you.

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:45

    It probably means ''Internal Peripheral'' (as input). Each pin can have 2 input functions. If the IP is disabled, then the input is just a GPIO. If the IP is enabled, then the internal peripheral (see the data sheet, not the reference manual) is connected.

    It might also mean Intellectual Property, since many chip manufacturers license designs from other companies for peripherals, and they tend to call this peripheral a block of ''IP''. But that is probably a bit obscure. For instance, Bosch licenses their CAN hardware as ''IP'' to chip manufacturers such as Silicon Labs.

    To add confusion, the data sheet calls this Alternate Input.

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:45

    Hi,

    I am not able to write and read from flash. I am suing M25P64 flash connected on SSP0.

    This sample code shows everything.

    I am using STR910 evalutation board. M25P64 is flash on board.

    I am able to read only Flash ID.

    Please find my code below. Suggest me if any mistake..

    Thanks

    arnaudAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:45

    Hello,

    Actually, if i replace GPIO_IPConnected_Enable by GPIO_IPConnected_Disable,in P2.4 and P2.5 configuration, the SSP0 can receive datas.

    I had the same problem with the CAN and the UART reception and the problems are solved with the same way.

    Best regards,

    Arno