Skip to main content
Visitor II
October 23, 2003
Question

Problem with ST7LITE05 Watchdog Timer

  • October 23, 2003
  • 3 replies
  • 700 views
Posted on October 23, 2003 at 12:09

Problem with ST7LITE05 Watchdog Timer

    This topic has been closed for replies.

    3 replies

    Visitor II
    October 20, 2003
    Posted on October 20, 2003 at 12:11

    1) I configured the MCU for hardware WDT and no reset on Halt

    2) Before executing the Halt instruction I wrote this code:

    bset LTCSR,#0; Clear Watchdog Timer

    halt

    3) After reset vector fetch I wrote this code:

    .main bset LTCSR,#0; Clear Watchdog Timer

    4) When the MCU is stucked and the WDT resets it I can see in the scope in the external reset pin(3) the reset pulse of about 30 us and then it is released for about 45 us. I suppose it belongs to the internal reset 256 Tcpu + the Vector fetch time and then the low reset pulse again.

    5) The MCU fails to wake up in normal mode because the WDT is not fully cleared and I don't know what else I have to do in order to assure the WDT won't reset the MCU immediately after RESET sequence.

    bset LTCSR,#0; Clear Watchdog Timer

    seems not to be enough for this purpose even before entering Halt mode and after Reset vector fetch

    Thanks

    Claudio
    Visitor II
    October 22, 2003
    Posted on October 22, 2003 at 14:59

    Did you clear the WDGRF Flag after the Watchdog Reset.

    If you have not cleared it, this could be the reason why the microcontroller is immediately reset again.

    I hope this helps.
    Visitor II
    October 23, 2003
    Posted on October 23, 2003 at 12:09

    The only thing required is to refresh the watchdog counter before entering into the halt mode; So make sure it is done