I have a problem, feature ‘s devices are: 1) ST9 HDS2V2 EMULATOR 2) ST92F120EMU presented on the board Emulator and Computer are linked by parallel port LPT1 In the PC there is like O.S. Windows 2000 Service Pack 4. Effected operations: I start the emulator and it come is a state of: (lighting of LED) POWER, EMULATOR RESET, ST9 RESET I start the program WGDB9 DEBBUGER and the emulator come in a state of RUN of course only the LED remaines alight showing the POWER. The PC answeres with the following window: ST9+ Debbuger : ->>ST9+ can't enter monitor mode ->> Reset the emulator! I press OK The program is opened with another window whose title is WARNING having the same message as before Please help me!!!