Skip to main content
Visitor II
May 31, 2006
Question

problem with str71xdemo_usb.axf

  • May 31, 2006
  • 6 replies
  • 1032 views
Posted on May 31, 2006 at 05:36

problem with str71xdemo_usb.axf

    This topic has been closed for replies.

    6 replies

    jmartin9Author
    Visitor II
    May 18, 2006
    Posted on May 18, 2006 at 13:38

    hi!!!

    I use EvalBoard MB393 and STR7 RVDK Realview debugger 1.7 and i tried to donwload the file :''str71xdemo_usb.axf'' but this message occured:

    Error: Unable to write Program memory at 0x0000

    Error S10000 (Server): Unable to Write at 0x0000 - Uknown Flash memory

    Error S0025 (Server): Unable to write memory at specified addr while Loading File.

    ________________

    Attachments :

    RVDG.PNG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtOi&d=%2Fa%2F0X0000000aPR%2F41A0buUzya7obqd0SxWD9o8yfm.2i2AaqVPnc6oR5P0&asPdf=false
    jmartin9Author
    Visitor II
    May 19, 2006
    Posted on May 19, 2006 at 07:52

    hi!!!

    this file was downloaded from the str7 page :

    STR71x Demonstration Software for MB393 board

    http://mcu.st.com/mcu/download2.php?file=1080747744.zip&info=STR7%20Software%20STR71x&url=/mcdfiles/1080747744.zip

    I use RVDK 2.1 for ST with Realview ICE.

    The only .axf that I can use is :

    str71xdemo_gp.axf

    If you know how to repair it, it would be nice

    jmartin9Author
    Visitor II
    May 19, 2006
    Posted on May 19, 2006 at 12:49

    It worked once :

    str71xdemo_usb.axf was loaded (with SW 13 14 15 as you said)

    (so as str71x_extflash.axf)

    I don't know with this worked at this time

    I plugged the USB cable and the board was recognized as a mouse by windows.

    However, nothing happened on hyperterminal when I hit a d w x (azerty or qwerty ?)

    The problem is I cannot reload both axf files in order to retry the demo.

    How to restart from a clean config ?

    - Do I have to load str71xdemo_gp.axf in internal flash ?

    - is a reset to do to load USB demo in external flash

    - ...

    Thank you for your help,

    jmartin9Author
    Visitor II
    May 23, 2006
    Posted on May 23, 2006 at 14:47

    hi!!!

    thank you for your help, we succeed to run the usb demo.

    1) However, both .axf files (demo_usb and extflash) need to be loaded with :

    SW15 opposite CPU

    SW13 opposite CPU

    SW14 toward CPU

    (both need to be loaded in RAM)

    2) Then Go (F5) until RAM is transfered into external flash.

    3) Run Hyperterminal (9600 8, N, 1) (serial cable on UART0)

    4) The boot switches :

    SW15 = opposite CPU

    SW13 = opposite CPU

    SW14 = opposite CPU

    5) Reset MB393 board =>

    STR7 HID Mouse Demo

    appears on hyperterm

    6) connect USB cable =>

    USB configured

    'a'

    'd'

    'w'

    'x'

    appears on hyperterm

    7) it works!

    now I would like to know how erase the external flash on the MB393 eval board?

    Thanks,

    jmartin9Author
    Visitor II
    May 24, 2006
    Posted on May 24, 2006 at 10:53

    hi!!!

    thank you for your help, i succeeded to erase the external flash.

    jmartin9Author
    Visitor II
    May 30, 2006
    Posted on May 30, 2006 at 12:22

    hi!!!

    i would like to know if it's possible to obtain the source code of usb_demo?

    thanks,