Skip to main content
Visitor II
May 13, 2004
Question

Problem with STVD7 2.5.3

  • May 13, 2004
  • 4 replies
  • 983 views
Posted on May 13, 2004 at 08:15

Problem with STVD7 2.5.3

    This topic has been closed for replies.

    4 replies

    adibAuthor
    Visitor II
    May 5, 2004
    Posted on May 05, 2004 at 08:54

    Hi,

    When debugging my application and placing a breakpoint somewhere in the code, the application stops and everythning is ok. If I remove this breakpoint or add a new one and then continue (F5 button) to run the application it doesn't resume (in the left down corner it shows ''Runing'').

    I have to restart the application using the (Ctrl+F5) button.

    Any Ideas??

    Visitor II
    May 10, 2004
    Posted on May 10, 2004 at 13:21

    Hi,

    Can you tell which micro, which version of the toolset and which debuging target you are using ?

    Without those information we can't help you.

    Regards
    adibAuthor
    Visitor II
    May 13, 2004
    Posted on May 13, 2004 at 06:09

    Hi,

    I am using ST72F264G2 on the IDB-ST72F264 evaluation board I wirte in ASM.

    I would like to add that my software is runing on external interrupt and does almost nothing in idle.

    Visitor II
    May 13, 2004
    Posted on May 13, 2004 at 08:15

    Hi Gilat,

    the problem happens because, after have reached a breakpoint and have modified it, the program runs in step-mode. Therefore you are no more in real-time mode.

    I suggest you to not change/add breakpoints after the code has reached it, this will mantain the real-time condition. For more information read page 7 of the inDART-STX for ST7 User's Manual Addendum, provided with the inDART-STX installation package.

    Regards,

    Nicola

    [ This message was edited by: Nicola on 13-05-2004 11:47 ]