Skip to main content
Visitor II
December 28, 2006
Question

Problem with UART in MCBSTR9 Board

  • December 28, 2006
  • 8 replies
  • 1209 views
Posted on December 28, 2006 at 05:31

Problem with UART in MCBSTR9 Board

    This topic has been closed for replies.

    8 replies

    nanuradhaAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:34

    hai,

    i am writing some data in the UART->DR register, but it is not same what i wrote. data what i send is 0-0F, but i am getting..... FF,FD,FB,FB,F7,F5,F7,F7,EF,ED,EB,EB,EF,ED,EF.

    i don't know why it behaves like this.

    here i am sending my code and expect sugessions.

    PLEASE HELP REGARDING THIS.

    REGARDS

    RAJ.

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:34

    hi raj,

    to test the end of write you are using the flag

    UART_FLAG_TxFIFOEmpty.

    you have to check the right status register,

    something like

    UART_FR & (1<

    or

    UART_FR & (1<

    ciao

    nanuradhaAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:34

    hai Stevejamal,

    in my program i want to transmit the data to the data register and monitor it on the hyper terminal. for this i have prepared the following code.

    UART0->LCR = UART_WordLength_8D | UART_Parity_No | FlowControl_None

    & UART_StopBits_1 & UART_FIFO_Disable;

    UART0->CR = UART_Mode_Tx | UART_Mode_Rx | 0x0001;

    com_baudrate (115200);

    for(i=0x0000; i<=0x000f; i++)

    {

    UART0->DR = i;

    while(UART_FR & (1<

    GPIO7->DR[0x3FC]= UART0->DR;

    for(j=0;j<=0xfff;j++);

    }

    while(1);

    }

    in my code i just put the data on the UART0->DR.

    but it is not same what i wrote. data what i send is 00-0F, but i am getting..... FF,FD,FB,FB,F7,F5,F7,F7,EF,ED,EB,EB,EF,ED,EF.

    if i send 00(0), then the data on UART)->DR is FF(1111 1111)

    if i send 01(1), then the data on UART)->DR is FD(1111 1101)

    if i send 10(2), then the data on UART)->DR is FB(1111 1011)

    if i send 11(3), then the data on UART)->DR is FB(1111 1011)

    if i send 100(4), then the data on UART)->DR is F7(1111 0111)

    if i send 101(5), then the data on UART)->DR is F5(1111 0101)

    if i send 110(6), then the data on UART)->DR is F7(1111 0111)

    so like this i am getting data. in hyper termioinal i am monitoring the related ASCII values.

    when i Debug my code i have observed these values in data register.

    from these values what i observe is my data is there, but it is ORing(|) with FF and Previous value.

    one more point is.. in my code i have enabled both TX and Rx (UART_Mode_Tx, UART_Mode_Rx)when i debug,i can monitor the data in UART0_DR as well as Hyper Terminal(ASCII Values).

    but if i enable only Tx then i can monitor the data in Hyper terminal (ASCII Values) but not in UART0_DR Register.

    i don't know why it behaves like this.

    its wonder that if u will help regarding this.

    thanks in advance.

    raj.

    [ This message was edited by: anuradha on 22-12-2006 11:06 ]

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:34

    I see that you use

    UART0->DR = i;

    while(UART_FR & (1<

    bit7 is TXFIFO empty

    when you send a char the fifo is not empty!

    Your code fill the fifo without any check on

    fifo full.

    In my opinion is better to use

    while(UART_FR & (1<

    the DR register is shared with RX and TX.

    if you have LOOPBACK enable you are able to see what you

    are sending reading the DR register.

    nanuradhaAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:34

    hai Stevejamal,

    when i enabled the loop back i can able to watch the data in UART->DR.its cool. but when i have enabled only Tx and send the data to the hyperterminal, then i could not watch the data on hyperterminal and

    UART->DR register. can u please send me the working example of UART.

    here my code is:

    UART0->LCR = UART_WordLength_8D | UART_Parity_No | FlowControl_None

    & UART_StopBits_1 & UART_FIFO_Disable;

    UART0->CR = UART_Mode_Tx | UART_Mode_Rx | 0x0001;

    com_baudrate (115200);

    for(i=0x0000; i<=0x000f; i++)

    {

    UART0->DR = i;

    while(UART_FR & (1<

    GPIO7->DR[0x3FC]= UART0->DR;

    for(j=0;j<=0xfff;j++);

    }

    while(1);

    thanks in advance

    raj.

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:34

    hi raj,

    I didn't find the master and peripherals clock initialization

    in your demo.

    Could you check this settings?

    if you have a wrong internal bus clock the baudrate you are

    setting is not the ones you'd like to have.

    Let me know.

    nanuradhaAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:34

    Hai Stevejamal,

    i have configured Fpll to 48Mhz, Fmaster=Fpll,BRCLK=48Mhz, PCLK is also 48Mhz. i have configured all clock settings in Startup file.

    please find an attachment.

    thanks & regards

    raj.

    [ This message was edited by: anuradha on 27-12-2006 11:02 ]

    nanuradhaAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:34

    Hai Stevejamal,

    please send me the working example Project of UART .

    in my program i have configured 48Mhz clock for Fmaster, Fpll, Fpclk, Fbrclk(baudrate clock). already i have send u my code.

    expecting updations.

    thanks

    raj.