I programmed an application using STR710F. On my board I use internal and external flash. I started it 2 weeks ago. When I came back the system has stopped. I debuged my application and has the following behaviour: The program runs with my emulator. The program runs in externla flash. The program doesn't run in internal flash. I made some tests and found out, that the program runs in internal flash only when the CPU speed (RCLK) is less than 18MHZ. I initialize the clock as followesn (oscillator frequenc is 14,7456MHz): case en44_2368: RCCU_Div2Config (ENABLE); RCCU_RCLKSourceConfig(RCCU_CLOCK2 ); RCCU_PLL1Config(RCCU_PLL1_Mul_12, RCCU_Div_2); while (RCCU_FlagStatus(RCCU_PLL1_LOCK) == RESET); RCCU_RCLKSourceConfig(RCCU_PLL1_Output); The system runs until the line RCCU_RCLKSourceConfig(RCCU_PLL1_Output); Than it stops. When I link these functions into external flash the system runs until next function in internal flash is called. However when I use an RCLK < 17MHz the system runs in internal flash. And it runs when I started my application two weeks ago with RCLK=44Mhz. By the way. I can program the internal flash within using my own bootloader (bootloader is executes in external flash) without any problems. Has anyone an idea why I can't execute the application in internal flash with RCLK = 44MHz?