Skip to main content
Visitor II
December 19, 2006
Question

problems with STVD

  • December 19, 2006
  • 2 replies
  • 742 views
Posted on December 19, 2006 at 14:36

problems with STVD

    This topic has been closed for replies.

    2 replies

    dlombardoAuthor
    Visitor II
    December 19, 2006
    Posted on December 19, 2006 at 10:39

    Hi, I have not the administrator privilege on the PC where the Softec Microsystem ST7 toolset (v. 3.00 based on STVD 3.1.0) is installed.

    When I try to open a workspace, the tool search for application file ''*.exe'' files instead of workspace file ''*.stw''.

    Choosing the option ''all files'' (*.*), the workspace is founf and opened, but the debug does not work.

    Entering with administrator privilege, there is not any problems.

    Visitor II
    December 19, 2006
    Posted on December 19, 2006 at 14:36

    This is taken from the release notes for Visual Develop:

    Administrator privileges are required to install STVD7 and to connect emulators to the USB

    port for the first time. Power user or administrator privileges are required to run STVD7.

    Regards

    sjo