I'm using the ED3k3 board with a uPSD3334V-40U6 MCU. I have purhcased an expanded code limit upto 32kb. I'm running a simple message program that uses UART0 to transmit messages from a buffered queue. My program compiles fine, however, when I use my RLINK-ST JTAG to flash it over, I get the following pop-up window: ''OPI 51 Step is not over yet? Go on? YES or NO'' here's the disassembly code the program hangs at is: 01AB: 20 db 20h ; ' ' If I hit yes, the pop-up window comes back again, if I hit no, the program stops execution at some assembly instruction for code in the startup.a51: 01A3: 20D504 JB F0, 01AA I am using the default startup.a51 that was provided with a slight modification to SCON, SCON = 0x52H. I have checked to make sure all the environment variables are correct, I have already used the UART and the UART isr in a different project with same hardware and it works fine. In debugging, I found some instances where initializing some global and local variables (int) to zero causes problems. In some cases, if I comment out the initialization and leave just the declaration, then the pop-up window doesnt show. Is there an new errata sheet I should look into? I am a novice, any help is appreciated. thanks.