Skip to main content
Visitor II
May 30, 2007
Question

Program ST10R167

  • May 30, 2007
  • 3 replies
  • 1228 views
Posted on May 30, 2007 at 07:38

Program ST10R167

    This topic has been closed for replies.

    3 replies

    fabien2Author
    Visitor II
    May 29, 2007
    Posted on May 29, 2007 at 12:27

    Hello,

    I'm new and I have a question of beginner.

    So I have a ST10R167 and I wish to program it. If I have understood, this ic have an internal rom and I have already an ic programmed.

    Can I recover his program to send it in another empty ic ?

    If yes, which software could I use to ?

    Can I use the software st10flasher 2.4 ?

    Can I use a converter base DIL48/PQFP144 to program it (because I have

    a device programmer DIL48)?

    Is it possible that I cannot read the program (program locked in reading) ?

    In fact, I just want to copy/stick the program.

    Thank you for your answer.

    fabien2Author
    Visitor II
    May 30, 2007
    Posted on May 30, 2007 at 05:29

    Hello Neila,

    Thanks for your quick answer but I don't understand !

    Here it is the block diagram, and you can see just like me an internal rom

    takes part in the functional mode of the ST10R167-Q3.

    ST10R167 > R for ROM

    ST10F... > F for FLASH

    Could you explain to me ?

    Thanks.

    ________________

    Attachments :

    SurveyReport_1_.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0NN&d=%2Fa%2F0X0000000bYB%2FtvrzSGr90DQVqPhQkGMGrsZvO6yOLLIcfMH6M0XAeCg&asPdf=false
    fabien2Author
    Visitor II
    May 30, 2007
    Posted on May 30, 2007 at 07:38

    If I do understand this time the references has changed

    In the past the ST 10 R 167 was different

    because the block diagram I possess puts to light an internal rom

    and it's not the case any more. So the generic family ST 10 X makes now a difference with the last generation of chips.

    Is it all right if I replace now an OLD ST10R167 by a NEW ST10C167 ?

    And what would be the software to be used for programming it ?

    Thank you for your answer