I own a ST7-MDT-00-EPB2 and I need to modify the supplied user interface to program quite large quantities of the ST7LITE05 MCU.
Simple operators will do the job, placing a device into its socket and then pressing a single button will trigger the programming without any possibility from the operator to change any parameters or code of what they are programming. My question are: Is there any possibility to access the API set of the programmer software in order me to create my own interface. Is this API set available and well documented? I need only de programmer hardware and the low level PC software, I'll do the rest as far as the API is available. Third party programmer manufacturers are welcome also Claudio
If uou need to program a large quantity of ST7 devices, you can use the SofTec Microsystems MP8011A Gang Programmer. It can program up to 8 devices at time. More info at www.softecmicro.com
The MP8011A (gang programmer) doesn't support the serialization. The serialization is available on SofTec Microsystems inDART-ST7 series only (ISP programmer/debugger for ST7). Ciao, --Piero