Skip to main content
Visitor II
May 3, 2008
Question

Programmer for ARM Flash PSD, uPSD and DSM. Compatible with FlashLink

  • May 3, 2008
  • 1 reply
  • 720 views
Posted on May 03, 2008 at 08:40

Programmer for ARM Flash PSD, uPSD and DSM. Compatible with FlashLink

    This topic has been closed for replies.

    1 reply

    okuliczAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:52

    F-LINKcable is a cheap programmer/debugger for ARM microcontrollers STMicroelectronics family. It is compatible with FlashLink JTAG. Programmer is connected to PC through parallel port, connection with target circuit is done through 14-pin FlashLink standard or standard 20-pin JTAG connector by adapter added to programmer.

    Features

    - Supports STR91x, Flash PSD, uPSD and DSM ARM microcontrollers family from STMicroelectronics.

    - Compatible with FlashLink JTAG

    - Available free software: CAPS and PSDsoft express

    - 14-pin connector for target circuit and standard 20-pin connector by Adapter

    - Operates with target voltages in the range of 3 - 5.5 V

    - Supplied from the target circuit, no need for external power supply

    - Connection with PC through parallel port

    Supported devices

    - STR9 Family

    - Flash PSD Family

    - uPSD Family

    - DSM Family

    0690X00000603NqQAI.jpg

    http://www.propox.com/products/t_181.html?lang=en

    :o :o :o :o :o :o :o :o :o